MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSM VDD and VDDIO Usage

Hello,In my prospective application, I am trying to use the LSM6DSM and also achieve a very low power state.In my application, the host device will operate at 3.3V. The LSM6DSM could be supplied by 1.8V so that it draws the least power, see here: htt...

CMehr.1 by Associate II
  • 2932 Views
  • 3 replies
  • 0 kudos

Can LSM6DSOX FSM process accelerometer data at > 104Hz?

If my accelerometer ODR on the LSM6DSOX is set at 3333Hz and my FSM (104Hz) checks accelerometer norm for 3 samples (28.8ms) to see if it is below a certain threshold, does it check the accelerometer norm for 3 *FSM samples*?In other words, does the ...

OlaBola by Associate II
  • 807 Views
  • 0 replies
  • 0 kudos

IIS2DH Threshold, Duration and Activation settings and understanding questions Brief: Customer using IIS2DH, required to sense 5KPH / 3.1 MPH over 5 seconds before trigging interrupt.

Good morning. Up front I apologize if these questions are simplistic in nature but I just really want to make sure I am understanding the datasheet and implementing correctly. Below is the code I am using to init the sensor:int32_t snt_iis2dh_init() ...

0693W00000NsiacQAB.png

Resolved! How to read lis2hh12 Activity/Inactivity status over registers?

I set ACT_THS and ACT_DUR registers, so now the chip enters on low data rate mode (10 Hz) when no movement is detected. everything is fine to that point. I don't have access to INT1 and INT2 pins physically so I need to read activity/inactiviy statu...

CZorg.1 by Associate II
  • 937 Views
  • 1 replies
  • 0 kudos