Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Dear community,i have one more problem with my lis2dh12 project.So my sensor run in STREAM-TO-FIFO mode.After init. i can interrupt my sensor und get the right data.After some time my uC go into sleepMode (deinit i2c bus).When i trigger my lis2dh12 a...
I need to understand what is the right SMD footprint recommendation for LIS2DH12.Recommendations in TN0018 SMD guideline AN , ultra librarian recommended land pattern and footprint actually used in DIL24 adapter significantly differ from each other. ...
I'm working with lsm6dso for activity monitoring project. I want to record the acc and gyro data in the fifo and trigger an interrupt when the number of samples in fifo are more than the configured watermark. I already achieved to get the gyro data i...
The ios app request the upgrade to new firware version, but it's not avalaible on web site.
Fan rack condition monitoring with industrial sensor machine learning core --- 1/2I watched the reference video of and did the same, butThe ST BLE Sensor app cannot recognize the device.Is there anything that the version cannot be different from 2021...
Hello,i have a problem with my lis2dh12 acc sensor.I use the sensor in low power, 8bit with 100Hz and STREAM-TO-FIFO mode.After a interrupt, i read out all 32 FIFO reg and the INT1_SRC reg. These value look good. But when i trigger the interrupt agai...
As per the Release Notes (v2.4.0 / 5-Nov-2021) for HS DataLog CLI example, I could see executable and libs are present under directory Utilities/cli_example for Raspberry Pi 3B. I have also exported and set the shared library path using command.expor...
Are there any I2C communication timings available available. Trials seem to indicate device is performing clock stretching and only achieving 200kHz on returned data.FIFO usage. To reduce impact of I2C overhead, I would like use single axis mode on ...