MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DSL vs LSM6DSR with (Acc/Gyro) INT1 issue

Hi, We have a PCB design which used to have LSM6DSL and we were using ACC/GYRO data from the sensor. Since we switched to the new LSM6DSR chip the INT1 does not trigger (when data is ready) anymore even though the sensor should be similar config (if...

AHuta.1 by Associate
  • 1579 Views
  • 1 replies
  • 0 kudos

Resolved! UNICO Pedometer Regression tool "cannot open regression_tool.config" and "cannot generate configuration file"

I'm trying to use the UNICO Pedometer Regression tool in offline mode to analyze accelerometer data from the LSM6DSO32 accelerometer. I have followed the instructions from the UNICO user manual regarding data format:-file name data_steps138.txt-data ...

SPort.3 by Associate
  • 6960 Views
  • 3 replies
  • 0 kudos

LSM9DS1 16G scale issue

Hello, We have found a non-expected behavior of the IMU system LSM9DS1 when is set with an accelerometer scale = +-16g. To show our findings, it is presented below descriptions and diagrams of the tests.Firstly, two different devices were tested to c...

0693W00000SvYIyQAN.png 0693W00000SvYJ8QAN.png 0693W00000SvYJSQA3.png 0693W00000SvYJhQAN.png

Interrupt generation on INT2 pin of LIS3DH

Hello, I'm facing issues when enabling LIS3DH click interrupt, AOI1 and AOI2 interrupts on INT2 pin. These interrupts works fine on INT1 pin. Following is the flow I do to enable click interrupt on INT2 pin. register - 20h value - 119  //ODR 400Hz a...

ADani by Associate III
  • 1273 Views
  • 0 replies
  • 0 kudos

Resolved! LIS2DE12 : How to read only one new sample ?

Hello,I'm trying to understand the LIS2DE12 behaviour. First, there is no AN (Application Note), thus I used the one for LIS3DH which seems close enough.What I want is that my accelerometer wake up my stm32. This works. After that I just want to read...

SimonF by Senior
  • 4952 Views
  • 9 replies
  • 0 kudos