MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Detecting a short isolated event using lsm6dso32x

Hi,I'm trying to use LSM6DSO32X to detect a short (<5ms) event isolated by at least 100ms from other events (before and after). It's on the Y axis and with a threshold of 500mg. I'm not having any luck setting up a single TAP event or by using FSM. A...

IRogo.1 by Associate II
  • 1318 Views
  • 1 replies
  • 1 kudos

AIS3624DQ returning same vale on all three axis

Hi,I configured the AIS3624DQTR sensor by using standard driver given by ST on GitHub, I am able to set all parameter correctly but when I am trying to read X,Y and Z axis. It is returning same value on all axis and value is not changing by moving se...

Myada.2 by Associate
  • 1367 Views
  • 1 replies
  • 0 kudos

Content of LPS22DF i3c IBI payload?

I have an LPS22DF sensor connected via I3C. I can enable I3C in-band-interrupts (IBIs), and see the IBIs occur on data-ready events.I see the IBIs have a 5-byte data payload, but I can't find any definition of the data in this payload. Is this descri...

RoHS Exemptions 7(a) & 7(c)-I Remove Plan

Refer to the RoHS pack 22 Final report, RoHS exemptions 7(a) and 7(c)-I are possible to be expired on July 1, 2024. Could you please advise if STMicroelectronics has any plan to remove exemptions for the below parts? LD1117DT33TRSM15T100CASTPS8H100G-...

YYao.1 by Associate
  • 1846 Views
  • 1 replies
  • 0 kudos

Resolved! How does the LIS2DH accelerometer generate its clock, and what could be causing the sampling frequency discrepancy in its interrupts?

I'm working with the LIS2DH accelerometer and I'm trying to obtain acceleration data at a rate of 100 Hz. However, I've noticed that the accelerometer interrupts have a frequency of 99 Hz. Also this frequency changes if I use another accelerometer of...

ADelb.1 by Associate
  • 2551 Views
  • 3 replies
  • 1 kudos

STEVAL-MKI208V1K conecting to nucleo F401

Hello I want to connect to the STEVAL-MKI208V1K via STEVAL-MKIGIBV2 (conected those both togheter) , with Nucleo-F401RE. I conected pins as it is shown belowF401RE-> MKIGIBV2MOSI (PB3 -> SDAMISO -> SDOSCK -> SCLPWM/D6 -> CS3v3 -> VDDGND- >GNDI want t...

KDług.1 by Associate
  • 1692 Views
  • 1 replies
  • 0 kudos

Wrist tilt and "funny" data in FUNC_SRC2

Hi,I trying to get the wrist tilt working. I have used the example in AN5040 page 55.I using the simple example setup, nothing else is set. Write 20h to CTRL1_XLWrite 84h to CTRL10_CWrite 01h to DRDY_PULSE_CFGWhen reading the FUNC_SRC2 it always retu...

TStee.1 by Associate
  • 1257 Views
  • 1 replies
  • 0 kudos