MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PDM to PCM via DFSDM getting nothing but static

On the BL47E-IOT01A2 there are two mems microphones (MP34DT01) both connected to DFSDM1_DATIN2. I'm trying to extract the data from just one of those boards and convert it to PCM using a DFSDM filter. I've configured DFSDM Channel 2 to connect to PDM...

RBair.3 by Associate II
  • 1938 Views
  • 1 replies
  • 0 kudos

LSM6DSL Drift Specifications

Hello, ST engineers. I am working with a general purpose IMU for a tilt sensor application. I am observing some drift on the sensor while the device is off. I have heard that all IMU's can drift a bit, but I was under the impression that it would hap...

RBurg.2 by Associate II
  • 5157 Views
  • 5 replies
  • 0 kudos

LIS2DH registers saved before Power Off

Hello. I am using a LIS2DH board (STEVAL-MKI135V1). I use the STEVAL-MKI109V3 board and the UNICO-GUI app to configure the LIS2DH board. I configure it for Wake-Up system for X axis. So, I change the register for only enable the axis x and it works o...

javier by Associate
  • 854 Views
  • 1 replies
  • 0 kudos

Why I can´t connect the SensorTile.box to cloud ?

Facing some problems with the ST BLE Sensor App. Whenever I try to connect the device to cloud (Azure) it shows connection error ( in both android and IOS Phones).The SensorTile.Box I´m using is STEVAL – STLCR01V1

IBen .2 by Associate
  • 1032 Views
  • 0 replies
  • 0 kudos

How to slove the problem which the register's storage space of the ASM330LHHX is smaller than external sensor 's connected?

I connected the ASM330LHHX(STM sensor featuring a 3-axis digital accelerometer and a 3-axis digital gyroscope) and INA228(one of the TI sensors measuring the current and voltage) via the I2C interface. What's more, I want to read the data from the AS...

SWu.6 by Associate
  • 1043 Views
  • 1 replies
  • 0 kudos

Interfacing PDM digital microphones using STM32 MCUs and MPUs

Hi,At Application Note 5027: "Interfacing PDM digital microphones using STM32 MCUs and MPUs" it described how to connect PDM microphone to SPI I/F of STM32. My question is:at SPI I/F clock is active only when there is SPI transaction, how can I caus...

AShpi.2 by Associate
  • 2030 Views
  • 1 replies
  • 0 kudos

Resolved! Detecting a short isolated event using lsm6dso32x

Hi,I'm trying to use LSM6DSO32X to detect a short (<5ms) event isolated by at least 100ms from other events (before and after). It's on the Y axis and with a threshold of 500mg. I'm not having any luck setting up a single TAP event or by using FSM. A...

IRogo.1 by Associate II
  • 1311 Views
  • 1 replies
  • 1 kudos