MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS2DH FIFO stream mode configuration issues

HiI am using an IIS2DH accelerometer and set up FIFO. The configuration sequences are following the IIS2DH example in Github, see below// 25Hz, Low-Power Mode Disabled, XYZ enabledACC_Write_Command(IIS_CTRL_REG1, IIS_CTRL_REG1_INIT_25HZ);// High-Pass...

ISM330DLC gyroscope zero offset

Hello,Overview: STM32F4 talks to an ISM330DLC (SPI serial interface) using the ST library. (https://github.com/zephyrproject-rtos/hal_st/blob/master/sensor/stmemsc/ism330dlc_STdC/driver/ism330dlc_reg.c)Problem: I have 5 boards, device at zero level, ...

cbaron by Associate
  • 2543 Views
  • 3 replies
  • 0 kudos

Resolved! LIS2DW12 wake up interrupt or double-tap interrupt on INT2 pin

Hello all,I am using LIS2DW12 accelerometer for single-tap and double-tap detection. I also want to use the wake-up interrupt simultaneously, but when both these interrupts are enabled, double-tap and single-tap are occasionally missed because both t...

amtpjoy by Associate
  • 2040 Views
  • 1 replies
  • 2 kudos

STEVAL-STWINBX1: BleSensors App = Cannot Connect via BLE

I recently received the STEVAL-STWINBX1 and plugged it in out of the box and it worked fine.  There was a firmware update which I did successfully. Next, I downloaded FP-SNS-STBOX1 v1.5.0 to test it out.  As per the readme I imported the "STM32CubeFu...

WP by Associate III
  • 3343 Views
  • 2 replies
  • 1 kudos

STEVAL-STWINBX1 Data Not Displaying in STBLESensor App

Greetings all,Just received a STEVAL-STWINBX1 multisensor evaluation board and I was able to connect to it through STMCube32Programmer (Win64 version) and am trying to see the real-time sensor data from the iOS app (ST BLE Sensor v5.0.0 on iOS 16.5.1...

DJHyp by Associate
  • 1183 Views
  • 0 replies
  • 0 kudos

lps22hb i2c interface(erorrs)

Hello, We want to operate the LPS22HB pressure sensor with the i2c protocol. The pin legs of the sensor are connected to the SCL - SDA 4.7k ohm pull-up resistors. Sa0/GND   Csi / 3.3  RES / GND. This is how connections are made. This way we can't get...

Resolved! Accelerometer with the highest accuracy

Hello, could you let me know which is the ST 3D Accelerometer chip with the highest accuracy? There is no need for gyroscope, neither for magnetometer. Thank you,Dimitris

LSM6DSO32 activity/inactivity detection

Hi I want to implement activity detection using LSM6DSO32 sensor, I follow the application note given by the st microelectronics. In that document they provided register details but for me there is no interrupt is generated.Register configuration: 1....