MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OUTPUT FROM ACCELERATION SENSOR LSM303

I am using a LSM303DLHC and setting it up with:// CTRL_REG1_A (0x20) loaded with 0x27 = 00100111, 10hZ rate,normal power enable X,Y,Z onWrite_Register(ACC_I2C_ADDRESS,0x20,0x27);// CTRL_REG4_A (0x23) loaded with 0x40 = 01000000, big endian, +/-2gWrit...

BLegg by Associate
  • 1331 Views
  • 2 replies
  • 0 kudos

Resolved! lsm303agr magneto temperature offset

Looking in the example code for the lsm303agr I noticed a function:  /** * @brief Enables the magnetometer temperature compensation.[set] * * @PAram ctx Read / write interface definitions.(ptr) * @PAram val Change the values of comp_...

Egbert by Associate
  • 2236 Views
  • 2 replies
  • 0 kudos

Lis2dh12 behaviour of i2c peripheral while powered off

Hi.I'm currently working on an application where I have a lis2dh12 accelerometer sharing an i2c bus with another sensor. These sensors need to be turned off by cutting off the power on the Vdd line. I'm running into issues with communicating with the...

Jonki by Associate
  • 1337 Views
  • 0 replies
  • 0 kudos

Resolved! What are the transfer functions of LPF1 and LPF2 for LSM6DSOX?

I am interested in calibrating precisely the delay introduced by the filter chain (LPF1 and/or LPF2) of the LSMDSOX (or DSO/DSM - I presume they are the same). I have found the settling times in Table 13 of App Note AN-5272, which is a good start, bu...

lgi000 by Associate
  • 2116 Views
  • 2 replies
  • 0 kudos

I am using IIS3DWB accelerometer for condition monitoring. In order to offset DC I intend to use HP filter ODR/800 which gives me high pass cutoff 33Hz. I wonder how to capture frequencies for a range below 33.3Hz (equipment running at 1500rpm (25Hz)?

I intend to use IIS3DWB accelerometer for machine vibration monitoring. In order to offset DC I intend to use HP filter ODR/800 which gives me high pass cutoff 33Hz. I wonder how to capture frequencies for a range below 33.3Hz (equipment running at 1...

AGosw.3 by Associate
  • 1295 Views
  • 1 replies
  • 0 kudos

MKSBOX1V1 and SPBTLE-1S module

Hopefully someone can assist:I am using the ST EVAL-MKSBOX1V1 (aka Sensortile Box) and trying to set up the SPBTLE-1S for use with STM32duino. I tried to follow the instructions in the STM32duino pages (here: https://github.com/stm32duino/Arduino_Cor...

GEmel.1 by Associate II
  • 3413 Views
  • 5 replies
  • 0 kudos

Resolved! IIS328 how to get out of an I2C hang

I'm using a IIS328DQ on an I2C bus @400KHzEvery now and again, the part hangs up and won't talk to me.  The only way out that I've found is a power reset.Attempting to follow https://community.st.com/t5/mems-sensors/if-hang-up-i2c-interface-of-the-li...

RLee4_0-1687460642025.png
RLee.4 by Associate III
  • 3853 Views
  • 5 replies
  • 0 kudos