MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISM330DLC 3-wire mode

Hi ST,I have an custom board using the ISM330DLC but I'm having difficulty configuring it's primary bus for 3-wire SPI operation.According to the ISM330DLC datasheet register CTRL3_C (0x12) must set to 0xC for 3-wire primary bus SPI mode to be enable...

1.jpg 2.jpg
GnR by Associate II
  • 4818 Views
  • 8 replies
  • 1 kudos

IIS3DWBTR SLEEP Mode current issue

Im using IIS3DWBTR sensor with STM32L562 controller,getting the high current  almost 800uA at sleep mode while testing.1.What are the pin configuration we need to set ?2.what are the registers need to be configure?

nandhinis by Associate II
  • 6876 Views
  • 14 replies
  • 0 kudos

Resolved! IIS2DLPC accelerometer data conversion

Hi:According to the IIS2DLPC datasheet and STMems_Standard_C_drivers are as followshttps://github.com/STMicroelectronics/iis2dlpc-pid/blob/cb5a10d963790fbe8863d4fd9449f8e00ed3cb8a/iis2dlpc_reg.c According to the IIS2DLPC datasheet, it seems that the ...

Myles_0-1689730271516.png
Myles by Associate
  • 2073 Views
  • 2 replies
  • 1 kudos

Part Marking

Hi ST Team, Can you share the Marking code specification for the component: LPS22HBTR ? Thanks, a lot Enzo

enzo2 by Associate
  • 1382 Views
  • 1 replies
  • 0 kudos

Resolved! Difference between IMP34DT05 and MP34DT05-A

Hello,I'm currently choosing a microphone in ST range and I wonder about the difference between those 2.The only differences I saw on datasheets are application types but no technical differences.Can you explain why technically some microphones are m...

JulienD by Senior
  • 2294 Views
  • 2 replies
  • 1 kudos

LIS2DW12 fifo bypass-to-continuous mode

Hello,I am working on the LIS2DW12 accelerometer, and I need to use the bypass-to-continuous mode for the fifo buffer. The idea is that the accelerometer is in bypass mode when it is inactive and not moving. When the accelerometer is moving and activ...

Resolved! STEVAL NKI128V1

Hey there. I just got this 3-axis accelerometer. Can I use it with Nucleo board?Thanks!

STEAL-STWINKT1 live data reading

Hello everyone,i have STEAL-STWINKT1 board. It has some sensor on it. I want to see these data live on screen and save these values. I dont need to plot fft. How can i do that without using coding with hal libraries. Thank you

bcryhun by Associate II
  • 1290 Views
  • 2 replies
  • 1 kudos

Resolved! IMP23ABSU vs MP23ABS1

Does anybody know if there is any difference between these two MEMS Microphones. The IMP23ABSU does have some Ultrasonic characteristics, but my understanding is the MEMS mics would have ultrasonic bandwidth anyway.Thanks

JKing.3 by Associate II
  • 2129 Views
  • 2 replies
  • 0 kudos