cancel
Showing results for 
Search instead for 
Did you mean: 

IMP23ABSU vs MP23ABS1

JKing.3
Associate II

Does anybody know if there is any difference between these two MEMS Microphones. The IMP23ABSU does have some Ultrasonic characteristics, but my understanding is the MEMS mics would have ultrasonic bandwidth anyway.

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @JKing.3 ,

Their performances are pretty similar, the main difference is that the IMP23ABSU has been characterized in frequency response up to 80kHz (for ultrasound analysis, see AN5522) and it has been qualified for industrial applications, while the MP23ABS1 is recommended for consumer applications.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @JKing.3 ,

Their performances are pretty similar, the main difference is that the IMP23ABSU has been characterized in frequency response up to 80kHz (for ultrasound analysis, see AN5522) and it has been qualified for industrial applications, while the MP23ABS1 is recommended for consumer applications.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks Federica, that's useful information.