MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Gesture EVK 1.4.0 doesn't communicate with VL53L8CX

Hello,I have a problem with the Gesture Evaluation Kit v1.4.0(EVK from now on) in combination with Nucleo F401RE and VL53L8CX ToF sensor. After uploading the binary file that comes with EVK, the GUI app sees the comport that Nucleo is connected to, b...

VToma.11 by Associate II
  • 1612 Views
  • 1 replies
  • 0 kudos

Resolved! IIS3DWB ODR at selected bandwidth of ODR/4 on LPF2

Hello Community,I am unsure what the ODR will be for the IIS3DWB sensor when we select the bandwidth of ODR/4.Kindly suggest the relationships if available, I did not find any mention in the datasheet except for Table 45.Are there any setting to sele...

Chubs_0-1690607232220.png
Chubs by Senior
  • 2270 Views
  • 4 replies
  • 2 kudos

Not receiving valid PDM data from MP34DT06J

Hi,I have spent the last 2 weeks working on a project with the STM32F102CBT6 that includes the MP34DT06J MEMS microphone, but so far I have been unable to get it to output a valid PDM data stream. I have tried using both the SPI1 in master receive mo...

TomLillie by Associate II
  • 20049 Views
  • 8 replies
  • 0 kudos

B-l475E-IOT01A connection for unico GUI with LSM6DSOX

Hello,I am trying to develop an audio classification through a decision tree in unico GUI platform using the mlc for lsm6dsox. I have the B-l475E-IOT01A motherboard and I want to know if it is possible to use the sensor LSM6DSOX with this motherboard...

SRodr4_0-1690999603521.png
SRodr.4 by Associate II
  • 926 Views
  • 0 replies
  • 0 kudos

Reading bad data from LIS2MDL using 3-wire SPI

Sensor: LI2MDLMCU: STML072I am trying to read the who_am_I register (register 0xAF) with the 3-wire SPI setup, but it is returning the wrong data.Below is a screenshot of the transmission and the return from the LIS2MDL. The transmission's first bit ...

Cfaya1_1-1690604682247.png
Cfaya.1 by Associate II
  • 2428 Views
  • 2 replies
  • 0 kudos

Resolved! DRDY not returning low on AIS2IH

I am using the AIS2IH and polling the DRDY bit of STATUS to see when a new sample is available .  I am using single data (on demand) mode and ODR bit is set.  The spec sheet says that DRDY returns low after the high part of X,Y or Z has been read, bu...

Resolved! Multiple STHS34PF80 on I2C bus

I have an application that requires two STHS34PF80 sensors on the same I2C bus. I tried using N-FETs on the SDA lines to select between them but this doesn't work, not sure why. I will try the 3-wire SPI bus but I am not sure my current MCU API supor...

KWine by Senior
  • 2402 Views
  • 3 replies
  • 0 kudos

Resolved! IMU LSM6DSO FSM Settings

Hello Team ST,I would like to have your guidance on setting a FSM for wrist tilt application. At the moment, we use following FSM settings as per the code here.Link: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/v2.00/lsm6dso_S...

ASoni2_0-1690543414543.png ASoni2_1-1690543657397.png
ASoni.2 by Associate III
  • 1583 Views
  • 1 replies
  • 0 kudos