User Activity

We are using Murata LBEE5HY1MW  WiFi/BT module with a STM32MP157F based custom board, running OSD32MP1 Debian SDK v3.0 (Linux Kernel v5.10-stm32mp)LBEE5HY1MW module is connected to STM32MP157F via sdmmc3 (WiFi) and usart2 (Bluetooth) interface.Due to...
We are observing that LSM6DSV FIFO Timestamp is drifting at a constant rate when Gyro sensor is enabled.Our ImplementationWe are using 6-axis IMU sensor LSM6DSV with st_lsm6dsvx driver from ST GitHub and integrated with OSD32MP157 SiP.We've modified ...
The iNEMO inertial module LSM6DSRX supports sensor synchronization S4S for Qualcomm. Sensor data sheet mentions following S4S registers without much detail.S4S_TPH_L (04h) Sensor synchronization time frame register - low byte (r/w)S4S_TPH_H (05h) S...
We are using MuRata Module LBEE5HY1MW on our custom board based on OSD32MP157F. We are using Octavo Systems OSD32MP1 Debian SDK v3.0 based on Debian 11 and OpenSTLinux Kernel version 5.10.10.We've integrated following 1MW firmware files from murata g...
STM32CubeProgrammer v2.10, running on Ubuntu to flash a 64GB MicroSD card on OSD32MP1-RED board is successfull, but failed to flash 128GB MicroSD card on the same board. Same tsv file and image binaries are used. MicroSD Card is 128GB SanDisk Ultra M...
Kudos from