MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Anyone have v1.3.1 MEMS-STUDIO for download

Hi,We've been working on a project using v1.3.1 of MEMS Studio, but I've had to use a new laptop and it doesn't have this installed. Unfortunately, when I go to the downloads page I can only see v1.4.1 of MEMS Studio and it's forcing me to upgrade th...

SFowler by Associate II
  • 4046 Views
  • 9 replies
  • 0 kudos

Resolved! [LIS2DUXS12] MLC filter & results in FIFO

Hi,I can't find a way to select in MEMS Studio which MLC filters are passed FIFO and how to enalbe MLC result in FIFO.Configuration created by MEMS studio enabled MLC_FILTER_FEATURE_FIFO_EN in EMB_FUNC_FIFO_EN so I see selected MLC features in FIFO b...

tomny by Associate II
  • 305 Views
  • 4 replies
  • 1 kudos

Using X-CUBE-MEMSMIC1 without X-NUCLEO-CCA02M1

Hello, I am trying to record audio with external digital PDM microphones using the MEMSMIC1 example but it is not so straightforward without the nucleo expansion board. Because the CCA02M1 has a direct connection to the pc it is able to be detected a...

Resolved! [MEMS Studio] HPF feature bug

Hi,I've tried to use high-pass filter in MLC in MEMS Studio, but the results are incorrect for first windows in each data file. I found that result is different from the one from Unico, but probably because Unico just drops first 2 windows from each ...

tomny_0-1769093543815.png
tomny by Associate II
  • 219 Views
  • 1 replies
  • 1 kudos

Resolved! ISM330DHCX INT1 to LDO EN pins

I need to save power in a project; the system will turn on when shaken. I need to configure INT1 pin to leave the LDO open for 15-20 seconds. Conditions:1- Did the device move? (acceleration)2- Are the x, y, and z axes in the correct position?If cond...

YBAYR.1 by Associate III
  • 266 Views
  • 3 replies
  • 2 kudos

Resolved! LIS3DH footprint discrepancy

Hello ST Community,Based on a photo found on the internet of the LIS3DH chip and a comparison with the package information in the datasheet, I found a discrepancy in the footprint.The datasheet appears to show the pin-1 mark on the opposite side comp...

GALS_0-1769007094007.png GALS_1-1769007460878.png GALS_2-1769008479126.png GALS_3-1769008503511.png
GALS by Associate II
  • 233 Views
  • 2 replies
  • 2 kudos

Resolved! 9-axis sensor fusion implementation DT0058& DT0060

Hi Sir,1. Regarding Initialization (Absolute Orientation)In my application, I need to obtain an absolute orientation (Roll, Pitch, and Yaw) relative to the Earth's frame. Is my understanding correct that the Initial Quaternion must be computed using ...

TIENHUA by Associate III
  • 240 Views
  • 1 replies
  • 0 kudos

Resolved! lsm6dv320x odr-triggered mode not working

Hello, I'm trying to use ODR-triggered to get data aligned with my clock. I'm sending a square wave 50% duty cycle period 2000ms over INT2 pin, yet when I poll the IMU every 50 ms the accel and gyro data changes, even though it should be aligned to t...

rulmer_0-1769011277205.png
rulmer by Associate II
  • 219 Views
  • 1 replies
  • 0 kudos