MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Self test in IIS3DWB

What is self-test in IIS3DWB and what is the criteria to indicate pass or fail??

Aalekh by Associate II
  • 1832 Views
  • 3 replies
  • 0 kudos

Difficulty connecting to IMU sensor ASM330LHB

I am trying to connect the IMU sensor that is onboard the STEVAL_MKI236AA evaluation board. I am currently trying to connect that board to BeagleBone AI-64 or a basic arduino via I2C and was able to detect an I2C device as 0x6A and 0x6B as the board ...

Resolved! Setting sensor hub master i2c clock speed

Hi @Federica Bossi , I need help with setting LSM6DSO sensor hub i2c master clock speed. How do I set the master i2c clock speed between LSM6DSO and external sensor for sensor hub operation? Is there registers or something else on LSM6DSO that contro...

el659 by Associate III
  • 4296 Views
  • 8 replies
  • 0 kudos

LPS22DF OR LPS28DFW

Hello,I have question please, can you tell me the protection index (IP) of the LPS28DFW ? also the LPS22DF has 22000g High shock survivability, it's perfromant for my application but for the LPS28DFW i don't find any information on the datasheet abou...

ljm by Associate III
  • 3809 Views
  • 8 replies
  • 1 kudos

Resolved! LPS33HW and LPS27DFW

Hello,Please, for a pressure measurement in an environment of dust and humidity, which sensor between the 2 you recommend as well as what is the IP protection rating of each sensor.Thanks in advance

ljm by Associate III
  • 1365 Views
  • 1 replies
  • 0 kudos

LSM6DSL Self Test Thresholds

I have performed the self-test on LSM6DSL and observed that it was noted the thresholds mentioned in the datasheet I want to know how these values of  90mg > xxx < 170mg  & 150 dps> xxx <700dps measured?Why does the acceleration and gyro change when ...

RamanaKumar_0-1705576951766.png

LSM6DS3 FTH or FIFO_FULL flags used as ISR

Hi,I am using steval MKI160V1 coupled with pybv1.0 under microphyton (spi speed 525000bits/s).I'd like to get every samples from gyro and accel at 1666 hertz speed using interruption.I have configured lsm6ds3( whoami = 69h) to do so, but while I am f...

L77d by Associate II
  • 1553 Views
  • 2 replies
  • 0 kudos