MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STWIN Trigger reset button via USB or Firmware

Hi!I have a STEVAL-STWINKT1B sensor running the HSDatalog firmware. I am interfacing with it using an USB cable via linux and a modified version of the "cli_example" relying on the "HSDatalog.h" interface, which I am compiling using cmake. When runni...

MKlan.1 by Associate
  • 2561 Views
  • 2 replies
  • 0 kudos

Resolved! LSP22HB having trouble with ONE-SHOT mode

I am using the LSP22HB on an I2C bus. I can read the "who am i" register and get the expected value. I can also read various configuration registers and see the default values. So, I believe I am communicating with the device.I don't set any register...

chriskot by Associate II
  • 2328 Views
  • 3 replies
  • 0 kudos

Configuring STEVAL MK1221v1 with the black pill stm32f401ccu6

I have been trying to configure the steval mk1221v1 which is a breakout board for the lsm6dso32x imu sensor using spi 4-wire interface but can't make to work. I am not sure if i am making the right connections. I am sure I have connected the scl, sda...

Resolved! why IIS3DWB timestamp values are zero ?

I have timestamp counter enabled and batching to FIFO with decimation=1. I can see the timestamp values are interleaved with the accelerometer values, but the timestamp values are always 0 like this (this is SPI trace):22 00 00 00 00 00 0A12 32 F7 2F...

mete by Senior II
  • 2577 Views
  • 4 replies
  • 0 kudos

Resolved! LIS3DH Single/Double Tap Detection Current Consumption

Hi,We notice that LIS3DH accelerometer has multiple mode which can be utilized to be used on low power mode for single/double tap detection. Does single/double tap detection increase the current consumption stated on the data sheet/design tip?https:/...

Dillah by Associate II
  • 6267 Views
  • 11 replies
  • 0 kudos

Resolved! LSM303AGR gives weird values output of the accelerometer

Hi,I am using examples from the github repo to test accelerometer. I can read device id from both accel and magnetometer. Also I can read back the registers I set.  However, when it comes to read accelerometer, I read same values from all axis of the...

Resolved! LIS2DE12 mangles REG1 register

I'm attempting to use the LIS2DE12 in perhaps the simplest configuration: To directly poll the X,Y,Z registers as needed. I'm using the I2C bus. At this point, I've added some debug checks, so the current process looks like this: 1. On wakeup, I read...