MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unicleo gui not detecting IKSO1A2

Hello, I'm learning how to use stm32 hardware and how to program it and today i connect the X-NUCLEO-IKO1A2 to my board (Nucleo-GO71RB) and installed the inucleo software,  i did everythink like te st video said, but for some reason the software does...

Fxpires by Associate
  • 1603 Views
  • 2 replies
  • 0 kudos

Android HAL for LSM6DSOX sensor

Hello experts,I am using rock chip board with android 12 on it along with the sensor lsm6dsox connected on i2c2.I have added the driver and compile the Linux and then build android images.After booting I can see device is detected on i2c and probed s...

amol4394 by Associate
  • 1844 Views
  • 1 replies
  • 0 kudos

Resolved! STHS34PF80: No data

Hi,we have designed a custom board that includes a STHS34PF80 but after triggering a one-shot acquisition, the DRDY bit is never set and reading from the TOBJECT_x and TAMBIENT_x registers without waiting for DRDY only returns 0. We are interfacing t...

NorSen_42 by Associate II
  • 3028 Views
  • 5 replies
  • 0 kudos

LIS3DH工作模式问题

我想知道LIS3DH的三种工作模式是什么?我收到了两份文件,一份是高分辨率模式、正常模式和低功耗模式,另一份是关机模式、正常模式和低功耗模式。我比较了两种模式的寄存器配置。低功耗模式相同,第一个数据中的高分辨率模式与第二个数据中的正常模式相对应。你能给我一个关于这个问题的具体解释吗?

LSM6DSO timestamp for external sensor event

Hi @Federica Bossi , I have a question about timestamp and the external sensor event.According to the application note of LSM6DSO (image above), timestamp's register is written when main sensor or external sensor event occurs. I have no problem with ...

el659_0-1717492879373.png
el659 by Associate III
  • 1466 Views
  • 1 replies
  • 0 kudos

I3G4250D Read the temperature

Hello,I am using a I3G4250D gyroscope and would like read the temperature. Currently, I read 246 (in decimal) in my register 0x26.In two's complement, it is equivalent to -9.   Then I have to multiply by -1 so -9 * -1 = 9°C (I am not sure)But It is t...

TomBr_0-1718294480109.png TomBr_1-1718294511992.png
TomBr by Associate II
  • 1910 Views
  • 2 replies
  • 0 kudos

Issue with MotionDI library initialization

I have added Digital Inclinometer application of X-Cube-MEMS1(9.6.0) on stm32f777zit6 wherein I want to read the rotation(angle) from LSM6DSL device. I have added all the required component files and Motion_DI library to the workspace.Reference taken...

Alps by Associate
  • 1326 Views
  • 1 replies
  • 0 kudos

Output Data Error for lsm6ds3tr-c

would you please help to review the attached log and give some advice to customer?Thanks.Attached is the test log data, test conditions:1. The device is fixed on the desktop without moving or shaking. 2.2. The CPU reads the X/Y/Z data of the Sensor v...