Skip to main content
MSing.8
Associate II
June 14, 2022
Question

Nicla Vision board integration with STM32 based boards

  • June 14, 2022
  • 1 reply
  • 1751 views

I see Nicla Vision board having lot of potential but the board in and of itself cannot do enough.

In order to open its potential, it should be able to talk to existing STM32(STM32F407 for e.g.) based boards through either SPI or UART interface.

  1. Do we have some tutorial on how to talk between 2 boards?
  2. Nicla Vision is Arduino based. Do we have something (duino??) which helps any STM32 based board to be configured through Arduino IDE or similar? This will essentially open up Arduino environment lovers to use SMT32 based boards.
  3. Integrate ROS (Robotic Operating System) into STM32CubeIDE like a package for e.g. how there is TouchGFX, FreeRTOS software packages.
  4. Integrate Amazon Cloud based software packages into STM32CubeIDE like there is Microsoft Azure package.
  5. Enable Ubuntu on STM32 based platform through again STM32CubeIDE like how Raspberry Pi supports linux.

Sorry so many in the list but couldn't resist posting.

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
June 14, 2022
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.