MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Microcontroller for LIS3DH

Posted on March 12, 2014 at 10:28Couple of questions ...1.  I have typically seen LIS3DH paired with Cortex M3 for e.g. in most of the health/fitness monitors. Is M3 required or could we use a M0/M0+. In other words what is the uC bandwidth required...

vishal by Associate
  • 224 Views
  • 0 replies
  • 0 kudos

Need some information about LIS331DLH accelerometer sensor

Posted on March 06, 2014 at 11:08Hello, Please give me information about the following questions. 1. What is the sensibility of the LIS331DLH accelerometer sensor? 2. What is the minimum acceleration that LIS331DLH can detect? Is there anyone who ca...

mamun by Associate
  • 193 Views
  • 0 replies
  • 0 kudos

What does position signify in linux sysfs for LIS331DLH

Posted on March 04, 2014 at 17:58 There is a linux sysfs file for accessing data from LIS331DLH. cat /sys/devices/platform/lis3lv02d/position What does this actually retrieve. Cartesian co-ordinates? If yes, with respect to what...

kiran by Associate
  • 259 Views
  • 0 replies
  • 0 kudos

Measuring Dynamic acceleration using LIS2DH

Posted on March 03, 2014 at 08:43I have calculated Tilt/Gradient in Non-accelerated systems(System acceleration  = 0); How to measure Tilt/Gradient in accelerated systems.As MEMS will give the X,Y,Z component of the resultant acceleration(g and a )....

LIS3DH impact detection

Posted on March 01, 2014 at 10:23HelloI have read that impact detection functionality can be performed by LIS3DH. I am unable to find any information on HOW to configure the device for impact detection.Is it identical to ''click'' detection? If no -...

igor2 by Associate II
  • 216 Views
  • 0 replies
  • 0 kudos

Configuring LIS3DH

Posted on February 20, 2014 at 08:31I connected LIS3DH in the following way , but the device does'nt give the correct reading.          What is wrong with this configuration? Vin = 3.3V, SPI 4 wires. I configured the registers with the following str...

yohai by Associate
  • 419 Views
  • 3 replies
  • 0 kudos

Question about LIS3DH FIFO

Posted on February 12, 2014 at 17:44HelloI am trying to use the LIS3DH in FIFO Mode with Filter enabled.In this mode, the X-Axis, and Y-Axis values get some normal values (they oscillate between -10 and +10) but the Z-Axis value seems to have a bypa...

avieira by Associate II
  • 514 Views
  • 5 replies
  • 0 kudos

LIS3DH datasheet error?

Posted on December 16, 2013 at 14:53In LIS3DH datasheet (Doc ID 17530) on table 25 we can see: Default value 00     ODR3-0 (0000:50Hz Others:...) on table 26 we can see: 0000 Power down mode So what is ODR = 0000  Power down or 50Hz? #lis3dh

Mich1 by Associate III
  • 219 Views
  • 1 replies
  • 0 kudos