Resolved! stm32 RCC Register ?
While looking at the rcc registers, you can see the ICSCR register on the debug screen, but when I write on the program, I encounter an error, I wonder what is the reason.
While looking at the rcc registers, you can see the ICSCR register on the debug screen, but when I write on the program, I encounter an error, I wonder what is the reason.
I've grabbed the latest SVD files from https://www.st.com/resource/en/svd/stm32l4plus_svd.zip, and confirmed that the RTC section is incorrect. It contains an ISR register, as in an original STM32L4 RTC, but not the SR and ICSR registers as in the S...
I recently had to look at the SVD file for STM32F2 series chips, and found that the STM32F215.svd file contains entries for Ethernet and DCMI peripherals, even though that's the discriminating feature between them and the STM32F2x7 chips that they do...
STM32G0B1 MCU, System Viewer file STM32G0xx_DFP\1.3.0\CMSIS\SVD\STM32G0B1.SVD: The file does not contain a description of the peripheral modules ADC, COMP, EXTI, DMA, FDCAN, FLASH, RCC, SPI, USB and others. There is a description of only HDMI_CEC, CR...
I'm developing a project using the STM32H745 HSEM and found a couple problems with the svd file that make debugging more difficult. My contact with IAR suggested I share my finding with ST to see if a working version can be supplied. 1) The svd fi...
In the actual SVD file (ver 1.7) the Ethernet peripheral registers are incomplete, Ethernet_MAC section actually we have Ethernet DMA registers, and no register descriptions for ethernet MAC. Beside even the Ethernet_DMA registers are showing incorre...
STM32G473 svd file (used in STCubeIDE in SFR view) shows FDCAN message RAM as if it was another instance of FDCAN peripheral
Hi,I work for Analog devices and presently working to port the software from our hardware to the STM32L4S5ZI. I needed a file that is similar to the attached file which is for our device.Please let me know how to get this file for the STM32L4S5ZI. I ...
STM32CubeIDEVersion: 1.5.0Build: 8698_20201117_1050 (UTC)Project for STM32G071 (Nucleo), Bit names in SFRs wiev for DMA->ISR has wrong numbering.
DS, RM and Nucleo-boards are already available, but I couldn't find a SVD file for the G0 series.