Resolved! STM32L0x1 svd
Hi,I have STM32L0x1 svd v1.3, and it seems the PWR_CR LPSDSR bit is missing.Is there a more recent svd file? I can't seem to find it.Thanks
Hi,I have STM32L0x1 svd v1.3, and it seems the PWR_CR LPSDSR bit is missing.Is there a more recent svd file? I can't seem to find it.Thanks
I am facing a issue as follows " I am currently working on a project that involves integrating USB functionality for data transfer and data logging on an STM32F407VG micro-controller. Specifically, I want to log data files on an SD card and enable t...
Hello all,I am working with the LBAD0ZZ1SE module, also used on the B-L462E-CELL1.I successfully adapted the "Nx_TCP_Echo_Client" Sample from X-Cube_cellular 7.1.0 to fit my needs but right now am stuck at the final step, which is the low power mode....
Posted on December 06, 2017 at 10:13Hello,I used the STM32L073RZ and I used Stop mode for saving current.And my problem is when I measured the current consumption of this MCU, I found arround 3uA during only 3 minutes after starting the Stop mode an...
I am working on freeRTOS CMSIS V1 on a project. I am using STOP mode to reduce the power consumption (since the device I am making is battery driven). When entering the STOP mode, I noticed that freeRTOS task is still running at the background on a s...
I am trying to create a frequency meter in a STM32U575ZI microcontroller that works with ThreadX and low power consumption using the low power timers LPTIM3 and LPTIM4, as well as an interrupt using EXTI 14. In summary, I use LPTIM4 to count input p...
My system has my main thread, a System Timer Thread, and one called Idle that I suspect isn't really a thread. Part of my code reads commands from a UART and then acts on the command. While the code is waiting for the user to enter the next charact...
Hi, I'm reading the AN5496 - Rev 3. I'm confused by equation (6) and (7). If all they are the transfer function of the closed-loop system, why there are different?Thanks.
Hi all!I'm working with an STMF401CC chip, and all tools up to date as of today.Code generation calls above mentioned function in SystemClock_Config() in main.c.In stm32f4xxhal_pwr_ex.c this function clearly is not available for STM32F401 devices, bu...