STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! PH3-BOOT pin

I did pulled up pin PH3-BOOT high (3.3V). I tried simple code but it looks like it is sitting there and doing nothing. I get this error message. Most chips would have just BOOT pin one function not PH3-BOOT.Multiple errors reported.1) Failed to execu...

0693W00000aJmPBQA0.png
MNapi by Senior II
  • 906 Views
  • 7 replies
  • 0 kudos

Bad board or bad debugger?

Hi,I have a B-L475e-IOT01A1 board. I have been trying to learn FreeRTOS with this board. I am using STM32CubeIDE v1.12.1. When I simply load an application onto the board, it appears to load properly. However, when I try to run my code through th...

jmazz.1 by Associate II
  • 498 Views
  • 6 replies
  • 0 kudos

ST-Link Chipset

Does ST manufacturer a chip that allows integration into a project which provides USB to SWD for the additional ST32 chips? I would like to remove the need for an external programmer and just be able to add a preconfigured USB to SWD SW-Link bridge ...

JWill.10 by Associate II
  • 929 Views
  • 8 replies
  • 0 kudos

Failed to execute .localhost:61234

Hi, i have recently purchased an STM32F746G-DISCO.i am very new to STM and compontents, but my manager would like me to try and build an interest with it. I followed a tutorial online, and i have followed the exact routes but i keep getting this erro...

JLythgoe by Associate
  • 520 Views
  • 1 replies
  • 0 kudos