Certified RTOS for STM32
Hi,I have general question. What certified RTOS do you recommend for using in medical device running on STM32F/G/H that will be certified in accordance with IEC 62304 Class C?Best regards,KK
Hi,I have general question. What certified RTOS do you recommend for using in medical device running on STM32F/G/H that will be certified in accordance with IEC 62304 Class C?Best regards,KK
Hellois it possible for the microcontroller with USB OTG to download the program memory from the USB stick itself?In other words, change the firmware simply by connecting a USB stick with a .bin file and perhaps by resetting the component.So far I ha...
Hello everyone, the STL_programmer currently calculates the CRC only for the in-use memory or up to the binary file size. Is there a way to fill the remaining flash memory with zeros and calculate the CRC for the entire flash area, eliminating the ne...
Dear Community Members, While working on my current STM32F103 project and attempting to integrate the X-CUBE-CLASS-B Library, I've come across a potential issue in the file `stm32fxx_STLstartup.c`. Specifically, it concerns line 351: 351 if (STL_...
We will be submitting our STM32F101vft based appliance for UL certification. We found the self-test extension X-CUBE-CLASSB. I review app note AN4435, and also found this community post from Christophe Vrignaud helpful. The example project STM3210...
Hi,I run using the STM32CubeExpansion_Cloud_AZURE_V2.1.0 follow this Readme instruction.But why it stuck at the Writing Credentials to boards...
Hi,Currently, I am testing the authentication example using STSAFEA110 expansion board with X-NUCLEO-G474RE.I follow the steps in STMicroelectronics.X-CUBE-SAFEA1_GettingStarted.pdf and also compared the STSAFEA110 expansion board+NUCLEO-L476RG Authe...
Hello. I am a SW engineer who is developing an electric vehicle charger.The headquarters is developing a slow charger with the STM32F1(STM32F103RCT6) series and is preparing for MET certification.Looking to prepare for UL 1998 functional safety, I ne...
hI! I am using the LPTIM, but not work in 486us, the minimum value is 2.6ms. in the logic analyzer i view:
I'm using the STM32F767 MCU and Keil compiler. The Keil version is Fusa 16.2. When applying the STL library in the Keil compiler environment, a rom test failure occurs.STL version is 4.0, and it was applied as in the guide document, but STL_Lib respo...