STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1238 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 509 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Debugging program in external flash XIP mode STM32N6

Hi,I am trying to debug STM32N6 program loaded in external flash. When I started the debugger in the FSBL project I can put a breakpoint just before it jumps into application inside external flash. It is obvious I wont be able to see the symbols sinc...

sai2_0-1744868672813.png
sai2 by Associate II
  • 3925 Views
  • 6 replies
  • 5 kudos

Cannot then build the project. It just sits there

Split from STM32CubeIDE missing “STM32 Project” and CubeMX after fresh installation - that issue was resolved.This is a new issue.The new version 2.1.1 appears pretty useless even after trying to make a project with the separate cubemx. From the IDE ...

Rstuc.1 by Associate
  • 206 Views
  • 2 replies
  • 1 kudos

Unable to download the stm32cubeide

I am trying to download the windows version of the IDE but I can't get it to work. Either the download button doesn't do anything or it's just not there. I've tried with different email accounts, different web browsers, different networks but that di...

STM32CubeIDE and C++ support

Hi C++ Developers,   As you may know, developers downliading Cube tools from st.com will receive an e-mail asking them to provide feedback. From this feedback we see some complaints vs the C++ support in STM32CubeIDE. The complaints are however lacki...

Resolved! How to open ioc file inside stm32cubeide?

I do not know what happened. If I double-click ioc file, it used to open inside CubeIDE. But now it will open inside another separated cubemx window. I may have changed some settings by mistake.How to change the settings back so I can open ioc file i...

open2.png
snkparty1 by Associate III
  • 1649 Views
  • 7 replies
  • 0 kudos

Resolved! HAL drivers with STM32C5 and STMCubeIDE

Hello guys, I started a project using STM32C552RET6 and STM32CubeIDE. When I use the autocomplete feature to select a HAL function, I can’t find it. I have to type the function manually.Does anyone know how I can fix this problem?Thanks for your help...

STM32H747I-DISCO unable to flash in Ubuntu 22.04.5 LTS

Hi SupportI have experience in STM32 with Zephyr but I am trying out AMP for the first time.So I am trying out OpenAMP example from STM32CubeIDE. I can compile the example but cannot flash the same.I have the following errorThe ST-Link device is pres...

jo512_0-1775713970923.png jo512_2-1775714007951.png
jo512 by Associate III
  • 529 Views
  • 14 replies
  • 6 kudos