2026-04-12 10:37 AM - last edited on 2026-04-13 1:40 AM by Andrew Neil
Split from STM32CubeIDE missing “STM32 Project” and CubeMX after fresh installation - that issue was resolved.
This is a new issue.
The new version 2.1.1 appears pretty useless even after trying to make a project with the separate cubemx. From the IDE you cannot then build the project. It just sits there. I would hope that the IDE is at at capable of building and compiling the project but it appears that is no longer the case.
Did you employ someone from microsoft to break it. It was working perfectly before hand. New->STM Project->.....->build->debug.
I will revert back to 1.19 to avoid wasting more time and just use an older CubeMX as that was the only reason I upgraded
Please leave working software alone or simply improve it and not break it for no reason
2026-04-13 1:45 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results.
@Rstuc.1 wrote:From the IDE you cannot then build the project. It just sits there.
Yes, CubeIDE certainly should be able to build a project from Cube MX.
Did you follow the STM32CubeIDE 2.0.0 New workflow tutorial - as linked in that old thread?
2026-04-13 1:48 AM
Hello @Rstuc.1
It would be great if you could share your project.
I will be waiting for your feedback.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.