STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1617 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 607 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! No .ioc file generated; FPU not initialised

#include <stdint.h> #if !defined(__SOFT_FP__) && defined(__ARM_FP) #warning "FPU is not initialized, but the project is compiling for an FPU. Please initialize the FPU before use." #endif int main(void) { /* Loop forever */ for(;;); }Good mo...

Jad by Senior
  • 1111 Views
  • 3 replies
  • 2 kudos

Resolved! ioc file not generating

hi i have been trying to configure mcu of h745BIT3 208 pin, IOC file is not generating, and i have tried for g4 series same issue happening today only, is there any server down or update have to do.  regards,srinath

External memory loader on STM32H7R7I8T6

Hello,I am working on a project that requires the code to be stored in the external QSPI flash but the problem is, I have no idea how the external memory loader generated by CubeMX works. I have tried following this article, but the external loader l...

Kwame by Associate II
  • 1892 Views
  • 3 replies
  • 0 kudos

remove dependency from makefile

In an IDE makefile project I use a linker script which is created in the pre-build step. In v1.12 of the IDE it worked fine. Now I have to use 1.16.1 and now make complains at the linker step that it has no rule to create the linker script. Well, mak...

stryga by Associate III
  • 400 Views
  • 0 replies
  • 0 kudos

CAN bus able to read but not send message

Hello,I have a STM32F407G-DISC1 (a blue one, do not know if that matters), that I am using to prototype a system where I communicate via CAN bus to a boost recuperation machine, however I am not able to see my messages on the osciloscope, I am able t...

Asperagabriel_0-1752285434853.png Asperagabriel_1-1752285447908.png Asperagabriel_2-1752285464498.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.