cancel
Showing results for 
Search instead for 
Did you mean: 

Error on debug after repeated debugging sessions "Failed to execute MI command: monitor reset core"

Tobe
Senior III

Hi,

i never had to much trouble with errors while debugging. But its getting exessive.

It only happens, when i debug a session, after i had already debugged a session. It makes no difference, if i manually terminate the last session before. I already tried different reset methods, which seemed to have no effect either.

It only applies to starting the debug session with the "bug" button (which would include the rebuild).

Sometimes i have to restart the IDE to make it work again.

 

I never had such problems before, and i did not really change much with the settings.

This issue is not present, when using a Nucleo board, but there is another issue (hard fault on debug only).

 

I am using this: https://www.st.com/en/development-tools/stlink-v3mods.html

Bought from reichelt.de

6 REPLIES 6
Imen.D
ST Employee

Hello @Tobe ,

Did you try to update and use the latest ST-LINK driver?

Are you using an old Windows version?  CubeIDE is only supported Windows 10 and 11. So, if you are using an old Windows version this might affect the IDE functionality.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

I am using not the most updated drivers/IDE. But i cant remember it working that bad before, so i think there might be some setting that cause this problem. Or even some state when debugging?

Andrew Neil
Super User

@Tobe wrote:

This issue is not present, when using a Nucleo board


So what board are you using ?

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:
So what board are you using ?

Indeed.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Its a custom made PCB.

It works without issue on the first debug session. Where could there be the problem?


@Tobe wrote:

Its a custom made PCB.


So give full details - schematic, etc - as noted in the link.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.