STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1544 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Headless build: always building after clean

Hello, for static code analysis I need the output from the clean/build process. So I searched how to build my project via command line and found the headless-build.bat (I use windows 10). After some problems with the syntax I finally got it running. ...

KR51K by Associate III
  • 2041 Views
  • 2 replies
  • 0 kudos

SWV Exception Timeline Graph - How to use?

Hi!I created a simple project in CubeIde to try out this function.SWV Exception trace log works as it, but the timeline graph seems to me wrong.Belong the debug session a moving vertical red line appears on the graph, and nothing else.Could anyone he...

0690X00000DXG7pQAH.png 0690X00000DXG7fQAH.png 0690X00000DXG7QQAX.png
PTiha by Senior
  • 3133 Views
  • 6 replies
  • 0 kudos

problem of QSPI as flash memory and FMC as data memory.

hi...i want to make a project using QSPI external flash memory to run a code, and FMC SDRAM as data memory... how to do that? i have try FMC SDRAM as Data Memory example project from STM32F746-Disco FW package and debug it using external loader and c...

Lpria.1 by Associate II
  • 3502 Views
  • 3 replies
  • 1 kudos

Can a project built with STM32Cube IDE be Open Source?

Hi, i've built a project with the STM32Cube IDE, using standard HAL drivers and the USB middleware. Would like to open source it and share to others to use it, learn from it and modify it as like. Is this possible or ST licensing forbids this? I've r...