cancel
Showing results for 
Search instead for 
Did you mean: 

Change fixed(?) tiny font size in CubeIDE only in SMV ITM Data Console ?

UliAuer
Associate II

Hello guys !

I've got a question: I'm rather new to CubeIDE and I'm exploring the whole STM32 world with the help of some Udemy tutorials. I've also studied major parts of the CubeIDE manual. But I just can't figure out how to make the font size in the SMV ITM Data Console bigger....it's just so extremely tiny on my high res 32" display, and the commonly used shortcuts don't seem to affect this console but only the code editors and (strangely) the "normal" Console. Btw: The "Executables" view is also very small, but at least a little bigger than the ITM Console...

Could anybody help me here ?

And: In Disassembly view of Debug mode I can't see code line numbers (which DO appear in my tutorial....)...How can I toggle them on/off ?

Any help appreciated !

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Try use magnifier lens windows feature