STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1544 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 586 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

GUI Bug in CubeIDE

Look at the left part of screen. I don't know how to identify this block, but you can see that this is broken. It happens every time independently of my actions. I can not put debug pointers.

EL314 by Associate III
  • 2000 Views
  • 4 replies
  • 0 kudos

Issue regarding Nucleo-STM32F756 and STM32Cube

Hello,After using some different board on an existing code base, I went to upgrade to a F7 board. To test the new board I used the STM32Cube IDE, and small tests worked to validate part of my code base with the new board. To deploy continuous integra...

How to read RFID card using MFRC522?

Hello,I'm trying to read RFID cards using the Nucleo-F446RE and MFRC522. I've found this library, but it just always fails atfatal error: stm32f4xx_rcc.h: No such file or directory fatal error: stm32f4xx_gpio.h: No such file or directoryI've tried se...

XXien.1 by Associate
  • 1868 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE Debug Options

I'm using a STM32F401RE and developing on STM32CubeIDE.Since I have a Bootloader on address 0x08000000 and I had to move the Application to 0x0800C000 by changer the linker file:MEMORY{ RAM  (xrw)  : ORIGIN = 0x20000000,  LENGTH = 96K/* FLASH  (rx) ...

EGonc.1 by Associate II
  • 1060 Views
  • 0 replies
  • 0 kudos

CubeIDE debugger fails to load the binary - SOLVED

To end the horrible winter night... even the debugger fails in CubeIDE under Windows.On the same Windows machine CubeIDE can debug the same target in a Linux VM.Isn't it curious?Same error with OpenOCD and ST-LINK GDB server. Of course, Atollic just ...

0693W000007YzEoQAK.png 0693W000007YzF3QAK.png
Pavel A. by Super User
  • 2411 Views
  • 3 replies
  • 0 kudos