STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1413 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't update Cube IDE

I cannot run updates from within Cube IDE.Help>Check For Updates throws the following error dialog:Unable to read repository athttps://sw-center.st.com/stm32cubeide/updatesite1/.Unable to read repository athttp://sw-center.st.com/stm32cubeide/eclipse...

Dfarr.1 by Senior
  • 4821 Views
  • 5 replies
  • 0 kudos

CubeIDE strange presentation of nested folder structure.

See the image. I can't figure out how I have done this, but my source folders appear like this, rather than in a hierarchy. When I open the folders in explorer, they are all nested as you would expect, folders inside folders. They are not folders wit...

DJC by Senior
  • 1166 Views
  • 0 replies
  • 0 kudos

How to add the watchpoint?

Dear All: I am using the STM32cubeide,I want to toggle a watchpoint ,I choice a value,but can not triggle it:So how can i toggle the watchpoint?

0690X00000AqbG5QAJ.jpg
Raytheon by Associate II
  • 8487 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F746 Using TIM8 in Encoder mode is not working with Input capture on both edge ???

I need to run TIM8 on Encoder mode. My encoder has two channels (A and B 90 degrees), So I have used two channel TIM_CHANNEL_1 and TIM_CHANNEL_2 as encoder input (it will use encoder as a clock for TIM8) and my timer is working fine and CNT is updati...

MJ_1992 by Associate II
  • 2044 Views
  • 1 replies
  • 0 kudos

Resolved! Create Run and not Debug configuration

How can I configure a Run configuration for flashing that doesn't also break and throw me into the debugger? Note how all the relevant options in my Run configuration are greyed out. How can I enable them?

0693W00000DlXCaQAN.png

Resolved! Are the Systick registers correct in svd file for STM32g491?

In CubeIDE SFR view systick registers names do not match Programming Manual definitions.SFR:register | addressSTCSR  | 0xE000E010STRVR  | 0xE000E014STCVR  | 0xE000E018STCR   | 0xE000E01Cpm0214, page 246:register | addressSTK_CTRL | 0xE000E010ST...

TMark.14 by Associate III
  • 1313 Views
  • 3 replies
  • 0 kudos