User Activity

Hello,Is there a way to generate releasecode to release to the public without Debugging information in the File. But to debug the Code with some exta Debug Files later?I would like to build a seperate Hex/Bin and Debug file.In other IDEs or in GNU Co...
Hello,I´m working on a Project with a STM32F373CCT. I need to compensate the signal read from the SDADC Signal with the internal ADC Temprature sensor.The Problem is that I only get the Value 0xFFF from the internal Temprature Sensor and also the Ref...