STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1531 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 583 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! How to add .cpp and .h files to the project of stm32cubeide?

1) I added to folder Core/Inc file my_lib.h2) Added to folder Core/Src file my_lib.cpp3) I added #include "my_lib.cpp" to main.cppIn tmy_lib.cpp I have only one class for testing. This class works with PWM. When I compile project I get errors that su...

OMaka.1 by Associate II
  • 5654 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE V1.7.0, modulo arithmetic => Compiler Error?

Since 25 years I use functions or macros like #define usTimeRead() ((int16_t) (SysTick->VAL >> 1))   #define usTimePlus(TP, US) ((int16_t) TP - ((int16_t) US * (int16_t) 85))   #define usTimePast(TP) (((int16_t) TP - usTimeRead()) > (int16_t) 0)t...

ULehm.1 by Associate III
  • 11884 Views
  • 11 replies
  • 0 kudos

Resolved! CubeIDE 1.4 Hangs Using FreeRTOS

Hello everyone,I have Nucleo-L4P5ZG and the development environment is WIN10 , CubeIde1.4 and CubeMx 6.2.I am facing a strange behavior while I'm trying to debug a simple FREERTOS toggle Led code here are details:1- I started with Cube Mx and generat...

AShaban by Associate II
  • 3298 Views
  • 6 replies
  • 0 kudos

Why I can't manage embedded software packages in CubeIDE

I have downloaded and installed CubeIDE. My first question is : this is a combination of CubeMX and an IDE right? Anyway, I am trying to use Cube.AI and all tutorials talk about installing Cube.AI with CUbeMX not IDEAnyway I go to Help-> Manage embed...

STM32CubeIDE 1.7.0: No ST-LINK detected!

I know I'm not the first reporting such an issue here, but the "solutions" in the previous threads did not help.I yesterday have installed STM32CubeIDE 1.7.0 using the installer. When trying to run a code, a dialog opens saying "No ST-LINK detected!...

waldmanns by Associate II
  • 4818 Views
  • 4 replies
  • 0 kudos

Very newbe with microcontroller programming

Hello everyone!I'm start to learn MCU programming with STM32CubeIDE (have to learn by work).I've never programmed a micro before, so I'm a true beginner. I started with Youtube tutorials and learned how blink the led (by toggle, using the user button...

DMore.1 by Associate
  • 1819 Views
  • 3 replies
  • 0 kudos

Resolved! how do i change the driver?

I'm using NUCLEO-207FZGIn cubeIDE, HAL driver is provided by default.I want to change to the SPL(Standard Peripheral Library).Since I am a beginner, I would like to get tips. Before you try, ask a question.I wonder if it is enough to simply add the S...

Psang.2 by Associate II
  • 2032 Views
  • 2 replies
  • 0 kudos