STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1422 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Why my program doesn't compile using LwIP?

I'm trying to compile my program, but it doesn't work due to an error probably related to LwIP includes.In file included from c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.wi...

0693W00000ANAYJQA5.png
Jvan .10 by Associate III
  • 2182 Views
  • 2 replies
  • 0 kudos

Resolved! No such file or directory ?

Hi guys! I have a trouble about STMCubeIDE, I installed and created a project, Later, I received this two error ; c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.20...

bnymntrz by Associate III
  • 6960 Views
  • 3 replies
  • 0 kudos

Resolved! Weird STMCubeIDE debug behavior - global structs showing up as all zeros but the code acts as it they are populated with data as they should be!

I have a project on an STM32F4 that consists of a Bootloader and Main application. Both of these apps read an external Flash to retrieve configuration data. The Bootloader is looking to see if Main had previously uploaded new FW to the Flash and if...

MStra.3 by Associate III
  • 1364 Views
  • 1 replies
  • 0 kudos

STCUBE hogs whole screen width

Hello,I run an a laptop with an additional screen at the side. stcube starts up hogging all the available with and exact the middle, where there is a gap. Most other application behave more sensible. I would appreciate if stcube would do so too.

Resolved! STM32CubeIDE Black Theme Problem

I don't find any options to change the font color for some files like linker scripts (for C/C++ Files it's ok). It's very difficult to read the file and i would like to use the dark theme.Same thing for not included code : Maybe one of you is aware o...

0693W00000HoeQSQAZ.png 0693W00000Hof5QQAR.png
AdrienC by Associate
  • 3296 Views
  • 4 replies
  • 0 kudos

SDMMC on H7 using CubeIDE 1.8.0

Has anyone else had problems with the SDMMC peripheral on the H7 since the CubeIDE 1.8.0 Update. I have some old projects I went back to that had previously used this peripheral and now when mounting the SD Card I get a FR_NO_FILESYSTEM error. I have...

Jaboop by Associate II
  • 1696 Views
  • 2 replies
  • 0 kudos

How to input these instruments?

I tested the example "WiFiBasics" came from STM32CubeIDE on discovery board "B-U585I-IoT02A". The .elf file has been downloaded into board through STM32CubeProg, and when I opened PuTTY as it was told in example's "README", these was prompted:https:/...

MQi.1 by Senior II
  • 1181 Views
  • 1 replies
  • 0 kudos

How to convert MyLibName.a to MyLibName.bin?

Hello guys.I have an interesting project where I need to load user applications (binaries) from external flash memory (FATFS) into RAM and run them from there. Also, I want to use a static library (let's call it libAPI.a for example) that should be a...

0693W00000HnxjfQAB.png 0693W00000HnxkiQAB.png
Oleksandr by Associate III
  • 2582 Views
  • 5 replies
  • 0 kudos