cancel
Showing results for 
Search instead for 
Did you mean: 

C++ Support in STM32CubeIde - class symbol not accepted

Jens1
Associate

Hello All,

I made a C/C++ project with STM32CubeIde version 1.1.0. It works fine.

Then I added a C++ class by a cpp and hpp file. And tried to make an instance of the class in the main.c file. The compiler does not recognize "class" symbol in my hpp file. How to solve this?

Is there an coding example?

Thanks and regards,

Jens

arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32F429xx -c -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../Drivers/CMSIS/Include -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../Core/Inc -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"

In file included from ../Core/Src/main.c:25:0:

../Core/Src/CFlashLed.hpp:21:1: error: unknown type name 'class'

 class CFlashLed

 ^~~~~

../Core/Src/CFlashLed.hpp:22:1: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
KnarfB
Super User

A .c file is considered to contain C source code, not C++ and class is not a keyword in C. What you can do, is calling a C++ free function in a separate .cpp file from main() which in turn instantiates an object of you class.

ywang.1
Associate

rename main.c to main.cpp​