STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1534 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 585 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Switching from Debug to Release mode - how do I push firmware to target (beginner question, am I doing something wrong?)

I am beginner with STM32CubeIDE 1.8.0 and am having trouble delivering release mode firmware to the attached target (STM32F0Discovery module, which is otherwise working well.)I am now experimenting with switching from Debug (the default configuration...

wb0gaz by Senior
  • 14110 Views
  • 8 replies
  • 0 kudos

Resolved! Dual bootloader - how to?

Hi everyone!I have to implement a dual bootloader system on different stm32 microcontrollers in STM32cube ide, and I have some questions…The idea is the following:There is a “pre-bootloader�? at the beginning of the flash. When it starts, it gets som...

Resolved! How to add preprocessor symbol in STM32Cube IDE

#error "Define according the used Cortex core ARM_MATH_CM7, ARM_MATH_CM4, ARM_MATH_CM3, ARM_MATH_CM0PLUS or ARM_MATH_CM0"Based from this Topic https://community.st.com/s/question/0D50X00009XkXPtSAN/need-help-in-dsp-library-for-keil- The problem is so...

How do I configure an Rx only UART interface in cubeide?...

I dont want to 'waste' the pins on the Tx line as this will not be used (the datastream is one way from an RC receiver into the STM32) - This isnt a case of it being a half-duplex etc.I can set the direction of data to be receive only in the advanced...

JHoun.1 by Associate III
  • 3769 Views
  • 5 replies
  • 0 kudos

Beginner with STM32CubeIDE (1.8.0) installed (on Windows) and STM32F0DISCOVERY, want open/import "blink the LED" type example.

Completed firmware update at Help > ST-LINK Upgrade, so STM32CubeIDE is communicating with STM32F0DISCOVERY module.Now trying find a most-basic example (for example, the firmware present in the STM32F0DISCOVERY board would be a good start - blink LED...

wb0gaz by Senior
  • 2285 Views
  • 3 replies
  • 0 kudos