STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 587 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Problem with CubeIDE Update

I have two machines with Cube IDE installed. On one there is version 1.6.1 and the other is 1.7.0I want to update both to be able to open .ioc files from a college that has the 1.8.x The proxy settings are setup rigth because i am able to get the new...

0693W00000JPTaxQAH.png 0693W00000JPTYhQAP.png
Uloff.4 by Associate II
  • 1708 Views
  • 3 replies
  • 1 kudos

Resolved! Toggle led controlled by MFX_v3?

I am using STM32L496 discovery board and I want to toggle LD1 which is controlled by MFX_GPIO4 on MFX_v3 chip according to UM2160. I'd like to do this within STM32CubeIDE, but I am not clear how to manage the MFX expansion device properly. Is it poss...

Lsy.1 by Associate II
  • 1823 Views
  • 1 replies
  • 0 kudos

Resolved! Using STM32CubeIDE with ARM MDK builds

Hello, I created a Makefile Project in STM32CubeIDE which uses ARM MDK Toolchain. I would like to know if it is somehow possible to use STM32CubeIDE for debugging in conjunction with ARM MDK?As in uVision IDE from ARM doesn't support to load more tha...

LBöhm.1 by Associate III
  • 2980 Views
  • 4 replies
  • 0 kudos

ERROR: Couldn't parse external memory loader

Hi everyones,I have a little (but big) problem with customized external loader.The compiler report this error: " ERROR: Couldn't parse external memory loader"Stm32 Cubeprogrammer instead, tell me everything is OK.I tried to download a simple file ins...

0693W00000D0o2sQAB.jpg 0693W00000D0o37QAB.jpg 0693W00000D0o3lQAB.jpg 0693W00000D0o3gQAB.jpg
MPast.1 by Senior II
  • 3109 Views
  • 4 replies
  • 0 kudos

ADC Oversampling issue with STM32G474RE

Hi all,I am currently trying to implement ADC Oversampling so I can get 16-bit resolution of ADC result rather than 12-bit.the dual simultaneous mode is used for ADC, ADC1 and ADC2 conversion, and the following is my STM32CubeIDE Setup: ADC1 Ch 6 and...

0693W00000JOXafQAH.png 0693W00000JOXjDQAX.png
IJo.1 by Associate III
  • 11592 Views
  • 7 replies
  • 0 kudos

Resolved! I have an error of "multiple definition of `ProcessChar' I have the function ProcessChar() in two source files. There are no header files or prototypes that should make these functions global.

This is a project created with STM32CubeMX and then coding in the STM32CubeIDE environment.The error is in the linking process, but wondering why the linker should believe this function is defined twice by default. I had reason to believe these shoul...

Mike xx by Associate III
  • 3486 Views
  • 4 replies
  • 0 kudos