STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE Code Proposals not working

Hello everybody,I just recently installed CubeIDE on my Mac and Windows systems. On both Code Proposals for thinks like HAL functions or user defined functions does not work. Do you know if there's a chance to change that? I already activated all kin...

HReet by Associate
  • 3481 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 freezes when UART ringbuffer user bigger buffer

Hello!I'm receiving data by UART in a ring buffer. When my buffers are lower than 256 it works, but when higher, it get stuck in the first for loop of my code.This is my ring buffer.void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t ...

SGonz.2 by Associate II
  • 1917 Views
  • 2 replies
  • 0 kudos

Why duty cycle of I2C not 50% ?

Hi. I am using STM32L031 for my project. And I am using I2C to read eeprom. It is reading eeprom properly but if you see duty cycle on SCL(red one in the pic below), it is not 50%.My I2C spped is 400kHz. ON time I get is 750ns and OFF time is 1.96us....

0693W00000Nr14vQAB.png

Problem with undefined references in STM32CUBEIDE

Hello there,After an update off STM32CubeIde from 1.17.0 to 1.19.0, the compilation of my code generates a lot of undefined references in functions like HAL_Init(). Do you know how to solve this problem? All of the header files are linked in same C f...

EKama.1 by Associate II
  • 3205 Views
  • 1 replies
  • 0 kudos

Share code between Libraries

Hi, I need to support 6 libraries for 3-5 MCUs each, and recently I have struggled to keep up.Many users complain about bugs I thought I squashed ages ago, only for me to realize that I never updated the code for that specific MCU.Is there a way to s...

Ubus99 by Associate III
  • 2183 Views
  • 3 replies
  • 0 kudos