Question
How to resolve the error "CM4 Failed to read all registers" when trying to debug?
Hi, I'm tring to write my program on a Mikrobus Clicker 2 (STM32F407VG) from the Software STM32CubeiDE with a mac. then I create a project and connected my board on my ST-LINK/V2.
I configured Pins and set As Serial Wire. and the Debug As SWD.
I got this 2 errors (Alternate with same configuration):
ERROR 1 :
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : /Users/admin/STM32CubeIDE/workspace_1.3.0/myproject/Debug/st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Target connection mode: Attach
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J36S7
Device ID: 0x413
PC: 0xfffffffe
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 1.19 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
CM4 Failed to read all registers
FAILED to REGISTER Values from the target
Debugger connection lost.
Shutting down...ERROR 2 :
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : /Users/admin/STM32CubeIDE/workspace_1.3.0/alphaboxv2/Debug/st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Target connection mode: Attach
Target connection failed
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.What could make this error and how resolve it? What's CM4?
Thank you!