STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32F4 - HardFault_Handler / HAL_TIMEOUT errors

Hello!We have 2 identical custom PCB using STM32F446RE MCU, we encounter the following issues and we can't find out what is happening.I'll try to explain the best I can such problem, testing boards with simple LED blinking program:while (1) { HAL_...

C. Mart by Associate III
  • 12265 Views
  • 9 replies
  • 0 kudos

Resolved! I want to use stm32CubeIDE's GCC compiler to compile my project, but the program takes up too much Flash space

The optimization options for GCC compilation are: Optimize for size(-Os),The compiled result is as follows: The size of MCU Flash resources occupied is: text+data = 47264 Byte The.ld link script is shown below: Question: In my program, the....

0693W00000SwIogQAF.png 0693W00000SwIpoQAF.png 0693W00000SwIq3QAF.png
Lucky Dog by Associate III
  • 5720 Views
  • 6 replies
  • 0 kudos

Hello Everyone, I'm trying to run the sample code given to me by the provider of our board and I'm having a problem when I try to build the project.

This is the sample error that pops up. How can I fix this? I'm very new to this so I'm not very familiar with this error. Hope that someone could help me with this. Tell me what else I need to provide so you can help me better./Applications/STM32Cube...

NPine.1 by Associate
  • 2831 Views
  • 3 replies
  • 0 kudos

Resolved! CubeIDE how to set offset for program?

I am making a DFU for stm32f4-discovery board.My DFU is using a project generated by STM32CubeMX V1.0. And It worked well with the program generated by the STM32CubeMX V1.0But when I worked with a project generated by STM32CubeIDE, I cannot make the ...

binhla by Associate II
  • 5420 Views
  • 4 replies
  • 1 kudos