STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1226 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 509 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32L476 comparator constantly generates an interrupt

Hi. I configured comparator with neccessary settings using CubeIDE and LL library and got next generated piece of code: COMP_InitStruct.PowerMode = LL_COMP_POWERMODE_HIGHSPEED; COMP_InitStruct.InputPlus = LL_COMP_INPUT_PLUS_IO1; COMP_InitStruct....

ARa.2 by Associate II
  • 2202 Views
  • 2 replies
  • 0 kudos

Resolved! Failed to enable Live Expressions. Connection failed

Can't enter into the debug mode on the development branch, but when I switch to master branch I can normally use the debugger. Difference between master and dev branch is minimal, and projects settings and debugging configuration is the same. I've tr...

0693W00000UoXLHQA3.png 0693W00000UoXK5QAN.png
DCind.1 by Associate
  • 6447 Views
  • 2 replies
  • 0 kudos

Want a Buffer to Buffer compression (.zip) library

Hi all, I am using STM32 F411 Discovery board and am facing an issue with compression, i tried different compression libraries (zlib, mzip etc) all are using File system, unfortunately the F411 Discovery does not supporting Local File system, my conc...

How to build headless inside a docker container

I've installed STM32CubeIDE inside a docker ubuntu image.If I start my docker-image and mount the folder with my source code (base directory is called 'primary' and hostmachine is a MacBook), and run this command:/opt/st/stm32cubeide_1.10.1/stm32cub...

JAnde.15 by Associate
  • 1404 Views
  • 1 replies
  • 0 kudos

Ethernet not working

Hello community, I'm usingSoftware:-STM32CubeIDE v1.10.1--STM32Cube FW_F4 V1.27.1Hardware:-STM32F4Discovery-PHY DP83848-RJ45I want to implement the Ethernet peripheral in the STM32F407 mcu with RMI mode without RTOS (via polling mode), and I used stm...

QSDFG.1 by Associate
  • 1138 Views
  • 0 replies
  • 0 kudos

[SOLVED] Pin triggered Timer-Delay (STM32G4 Timer2)

Hello,how do I have to setup the timer-2 so it create an one-shot delay on every rising edge (could also be falling, does not matter).This timing diagram indicates what I like to do, so I get an output-Event for the DAC and callback for an ISR(option...

0693W00000UoRIRQA3.png 0693W00000UoRIqQAN.png