STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How do I activate the FPU on F411?

I am using the F411 by CUBE IDE.I enable the CUBE's library of DSP and it was accomplished naive. Even after I inserted <include "arm_math.h"> the BUILD worked perfectly. But, after I copied one arm_FIR_filter_example from GITHUB, the compilation cha...

JSILV.2 by Senior
  • 10658 Views
  • 13 replies
  • 0 kudos

Resolved! STM32H745i-DISCO bricked no connection even with boot1

Hi, I have recently bricked my STM32H745i-disco board by turning off the m4 core within OB which had a bulk of my code. My board became unresponsive, the LCD turns white and the leds on the board light up but do not respond to the reset button. Stlin...

CChri.5 by Associate III
  • 7879 Views
  • 15 replies
  • 0 kudos

Resolved! Is it possible to debug a Makefile project into STM32CubeIDE

Hello,as the title suggests I would like to do step-by-step debugging on Makefile projects using STM32CubeIDE, however when I try to create the debug configuration it keeps showing an error message:Not able to get mcu targetReason:Build configuration...

Can I build for multiple targets on one STM32CubeIDE project?

I am currently working on a project that will use a STM32L452VET3 when the product is deployed. The PCB for the product is still being laid out, so in the meantime, I have a Nucleo board that has an STM32L452RET6 that we will use to develop and test ...

Tz.1 by Associate
  • 2027 Views
  • 1 replies
  • 0 kudos

Trying to view flash while debugging

I've used Keil for the last year - and they have a feature where I can view the flash memory while debugging (and even change it)I can't seem to find that with CubeIDE. Is there a way to see flash memory? I want to read/write and confirm it's there,...

UART WITH STM32L476

i was planning to do an experiment i need to insert two numbers and calculate the sum of that two inserted number. Then i need to see them in terminal. However i have confused a bit. Could anyone help me? I get stuck over here.  /* USER CODE END 2 *...

ACekm.1 by Associate II
  • 5474 Views
  • 11 replies
  • 0 kudos

Resolved! Cannot install Devstyle Darkest Dark Theme (solved)

Update: To get it to work, do a fresh install of the IDE, untick the CDT site in "Available Software Sites" (Help->Install New Software then "Manage"), and then install DevStyle from marketplaceSister issue on the Genuitec forum site: https://www...

0693W00000WKaVNQA1.png 0693W00000WKaVmQAL.png 0693W00000WKaW1QAL.png 0693W00000WKaWBQA1.png