STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Defining variable in assembly with STM32CubeIDE

I want to define a variable in assembly code and write it in R0 whit this code:__asm__( " var1 DD #123 \n" " ldr.w r0, =var1 \n" );but I have this error when compiling: "Error: bad instruction `var1 DD 123'"The compiler doesn't know...

Slh by Senior
  • 7037 Views
  • 10 replies
  • 0 kudos

Resolved! C++20 syntax is not being supported by STM32CubeIDE

I'm writing C++ code wih STM32CubeIDE. Version of IDE is 1.11.0 and it comes with arm-none-eabi-g++ version 10.3-2021.10 . The compiler has some of C++20 features and I'm using them in the code.The problem is some of them are not recognized by the ID...

0693W00000Y8JPbQAN.png 0693W00000Y8JQUQA3.png 0693W00000Y8JW3QAN.png
navidcity by Associate III
  • 7794 Views
  • 7 replies
  • 1 kudos

Why systick timer interruption is occurring correctly on a nucleoboard debug session but it is never ocurring when the same fw is on a same mcu based custom board?

I am stucked 4 days at HAL_systickInit part of a code that was generated by Cube MX. I'm using:CubeIDE 1.6.1HAL drivers firmware layerFreeRTOS Middleware Nucleo-F207zgCustom pcb (very simple circuit board --> write and read GPIO from 32pin connector ...

genisuvi by Associate III
  • 1756 Views
  • 2 replies
  • 0 kudos

Resolved! Is STM32CubeIDE including a simulator in the debug mode?

Hi,I am approaching for the first time with STM32nucleo board and I am using STM32CubeIde. The debug tool provides a simulator to test if the firmware is working properly? I mean a simulation tool like that of MPLAB IDE for PIC microcontrollers which...

Zenk91 by Associate II
  • 11509 Views
  • 4 replies
  • 0 kudos

Resolved! Measure VCC/Battery Voltage Without Using I/O Pin in stm32l010f4

I have a circuit with stm32l010f4 that has no ADC pin available because I am using them as digital GPIO, but I need to measure the battery voltage in my application, my question is if Vrefint can be used to make the measurement. I have already made t...

0693W00000Y8BXSQA3.jpg
jdo by Associate II
  • 7953 Views
  • 6 replies
  • 0 kudos

Does stm32cubeide debugger limit number of images to load?

Hi,I need to debug several axf files. In 'debug configurations' -> Startup, I added the axf files that contain debug information. It works fine but only up to 4 files. If I load 5'th file the debugger presents the message:"Failed to insert all hardwa...

ari_v2 by Senior
  • 1824 Views
  • 2 replies
  • 0 kudos

Using PE Micro universal and ST link for debugging STM32H7

I am using STM32H745BIT6 controller on my custom board and using STM32CubeIDE ver 1.11.I plan to use the PE micro universal debugger and ST link both alternately to program/Debug the controller. I already had setup the ST link in STM32CubeIDE v1.11 a...

ATank.1 by Associate III
  • 1628 Views
  • 1 replies
  • 0 kudos