STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Trying to print float value using stdarg.h file in CubeIDE

I'm using an STM32F4 mcu to receive data from a sensor. Now i want to print that same data which is in float. I've tried using functions like snprintf/sprintf but they give some error about linker flag. Now i've tried to add -u_print_f in the linker ...

IHiro.1 by Associate
  • 1394 Views
  • 1 replies
  • 0 kudos

Hey :) I am trying to flash my program onto my stm ucontroller but I get a libusb error message. Can you help me please?

I'm using STM32Ide. I installed pypy libusb1 and python3-libusb1 in the software manager of linux mint (I am using linux mint 19.2). I thought I need some libusb to solve the problem but I couldn't solve it. I couldn't find a guide. I want to flash m...

0693W000000XFPqQAO.png 0693W000000XFPlQAO.jpg 0693W000000XFPbQAO.jpg
Ykost.1 by Associate
  • 5605 Views
  • 8 replies
  • 0 kudos

undefined reference to `__fabs'

I want to use the intrinsic floating point absolute value function `__fabs` as noted in the compiler specific features in the armcc documentation.When I build my project using the following settings on STM32CubeIDE: I get an error saying undefined re...

0693W00000Y8SHHQA3.png
DLian.3 by Associate II
  • 3709 Views
  • 5 replies
  • 0 kudos

How can I use Clang-format in STM32CubeIDE

I was previously able to use Clang-format in my STM32CubeIDE environment by using the CppStyle 1.5.0.0 plug-in, but CppStyle 1.5.0.0 seems that it's no longer available in the STM32CubeIDE Marketplace. After a recent update, I am unable to use this f...

STM32Cubeide debugger displays wrong float values

In the debugger, I see float variables as 9e-39 or similar that is totally wrong.In the following example the correct value is 615.133911When passing to int it is 615, as expected.it may be a wrong configuration of the debugger float number formatHow...

JLope.11 by Associate III
  • 3290 Views
  • 4 replies
  • 0 kudos