STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1471 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE creating objects from a class source outside the project gives a compiler error. Also the constructor of this class is not called.

I created a simple class in a folder outside the STM32CubeIDE:class AT24C256Driver{public: AT24C256Driver(); float get_m_foo();private: float m_foo;};I added the folder to the "C/C++ generals - Paths and Symbols" property of the project.The AT24C25...

Ceedling and STM32CubeIDE arm-none-eabi/bin/ld warning: cannot find entry symbol Reset_Handler; defaulting to 0000000008000000

I am trying to create a first Unit Test with Ceedling/Unity/CMoke for my STM32CubeIDE project.The project has started building but getting an error:-----------Linking test_functions_STM32G474RB.out... /Applications/STMicroelectronics/STM32CubeIDE.app...

RPG by Senior
  • 7941 Views
  • 2 replies
  • 0 kudos

How to run regex in CubeIDE version: 1.11.0

Hello community. I have question. I would like to use regular expressions regex. It adds #include <regex.h> and tries to use the regcomp or regexec function. Unfortunately after compilation I get the error "undefined reference to regcomp". How do I g...

How do I change options for headless build? I want to enable converthex so I can output hex files for automated builds

I can use headless build using the following command:Linux:cd <my project path> /opt/st/stm32cubeide_1.11.0/headless-build.sh -import . -cleanBuild <my project name>/DebugWindowsC:\ST\STM32CubeIDE_1.11.0\STM32CubeIDE\headless-build.bat -import . -cle...

Resolved! Debug terminated immediately on start (Solved)

I had been debugging this program for some time with no problems. After making change to a header file to resolve a conflict, the debugger would no longer run. The program compiled , loaded and verified OK, but as soon as the debug perspective appe...

TJack.2 by Associate III
  • 5855 Views
  • 3 replies
  • 2 kudos

Getting error "Could not verify ST device" in CM4 core when debugging STM32H745I-DISCO board using SWD mode in Segger J-link.

I am working on following platform:Hardware - STM32H745I-DISCO board.IDE - STM32CubeIDE v1.10.1.STM32CubeMX v6.6.1-RC2.Embedded MCU package for STM32H7 v1.10.0.I am using SWD mode in Segger J-link for debugging. I am getting error "Could not verify S...

Akast.2 by Associate II
  • 5206 Views
  • 5 replies
  • 0 kudos

Trying to print float value using stdarg.h file in CubeIDE

I'm using an STM32F4 mcu to receive data from a sensor. Now i want to print that same data which is in float. I've tried using functions like snprintf/sprintf but they give some error about linker flag. Now i've tried to add -u_print_f in the linker ...

IHiro.1 by Associate
  • 1379 Views
  • 1 replies
  • 0 kudos