STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 589 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to launch makefsdata.c?

I always used perl script, maybe I need to somehow use makefsdata.c?I just don't know how to launch makefsdata.c?I have Debian 11 CubeIDE v.1.11.2PS - I hope it is automatically to generate to me a headers in my .shtml files!?!

DK.7 by Senior
  • 3465 Views
  • 2 replies
  • 0 kudos

STMCubeIDE how to include github source code?

I have downloaded source / header files from github and placed them in the /Driver folder on my existing project. I included them in the project properties. as you can see from pic it shows up under Project Explorer Includes section but it is greyed ...

0693W00000YAOLiQAP.png
SWenn.1 by Senior III
  • 3050 Views
  • 5 replies
  • 0 kudos

Resolved! Error: No editor descriptor for id org.eclipse.cdt.ui.editor.CEditor after installing anew compiler.

After installing a new compiler (9-2020-q2-update) with the Toolchain Manager I get the following Error.No editor descriptor for id org.eclipse.cdt.ui.editor.CEditorI am using STM32CubeIDE 1.11.0.I have tried to change the workspace or a fresh instal...

FRieb.1 by Associate III
  • 10219 Views
  • 7 replies
  • 0 kudos

Resolved! STM32L476 wake up source detection

Set Blue button(wake up 2) as wake up source and shut down. Press blue button will wake up system and print wake up source.With cube debugging environment, everything is fine. It shows wake up source is 2But after stop cube debugging, disconnect JP6 ...

XGao.2 by Associate II
  • 4605 Views
  • 4 replies
  • 0 kudos