STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1429 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32L476 wake up source detection

Set Blue button(wake up 2) as wake up source and shut down. Press blue button will wake up system and print wake up source.With cube debugging environment, everything is fine. It shows wake up source is 2But after stop cube debugging, disconnect JP6 ...

XGao.2 by Associate II
  • 4518 Views
  • 4 replies
  • 0 kudos

STM32 debug problem (There is no .elf file) - CubeIDE

Hi. Im using STM32F103C8T6 to interface BMP388 pressure sensor. I downloaded a example project file. When i trying to debug it using ST-LINK I'm getting unable to launch error.In debug configuration window im getting 'Project file does not exist' err...

0693W00000YABVLQA5.png

Error from debugger back end

While programming an stm32f446re in stm32cubeide 1.10, UART protocol caused me trouble as this errors appeared:1) Failed to execute MI command:-var-create - * UARTError message from debugger back end:-var-create: unable to create variable object2) Un...

jreis.1 by Associate II
  • 4249 Views
  • 5 replies
  • 0 kudos

Resolved! How to add new folders and get them compiled in CubeIDE?

Hi,I am trying to add new folders in CubeIDE and get them compiled.Taking STM32CubeU5 as an example.I imported a GPIO example, under the file tree, it will show:--include--Application --Startup --User--Drivers --BSP --CMSIS --STM32U...

dchen by Associate II
  • 4085 Views
  • 4 replies
  • 0 kudos