STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1413 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 557 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Build error

[main] Building folder: testtest [main] Configuring project: testtest [proc] Executing command: "C:\Program Files\CMake\bin\cmake.EXE" -DCMAKE_BUILD_TYPE=Debug -DPRESET_NAME=debug -DCMAKE_INSTALL_PREFIX=D:/test2/testtest/build/debug/install -DCMAKE_T...

0693W00000aJEhBQAW.png

Find function - where are the results?

I am looking for a find function over the whole project. While Ctrl+F seems to work only on the active file, the more advanced Ctrl+H should work over all files. The search function executes (green progress bar going to 100%) and the searched text is...

MBaum.7 by Associate III
  • 4516 Views
  • 5 replies
  • 0 kudos

Tried stepbystep (Intro to UART) from stm32 website, build and debugging are a success but keeps shutting down before even sending out "HelloWorld" to TeraTerm. What could be the problem?

Hi all, im a beginner on stm32 (currently using l703rz) to play with. I have tried the code from stm32 stepbystep (Intro to UART), the build and debugging are a success. The problem is that it keeps shutting down after debugging and would not send ou...

LGuan.3 by Associate
  • 3305 Views
  • 3 replies
  • 0 kudos

I have installed the STM32CubeIDE 1.12.0 from the STM32 official website onto Windows10 Pro. l met lauching error meesage.

I have installed the STM32CubeIDE 1.12.0 from the STM32 official website onto Windows10 Pro.D:\09DB> st-stm32cubeide_1.12.0_14980_20230301_1550_x86_64.exe /ncrcbut when i try to launch it above, l met error meesage.Error message: "Error! Can't initia...

SLee.41 by Associate II
  • 3131 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L433RBT6 with CudeIDE, the program jump to somewhere else if enable interrupt or stuck at HAL_init()

I am using the STM32L433RBT6 for some uart communication project.My pcb only have STM32L433RBT6, LDO, LED, UART related circuit.I am also using the Nucleo-L433RC-P (STM32L433RCT6 )for the development.The Nucleo-L433RC is working fine for the LED4 and...

JFung.1 by Associate III
  • 3196 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeIDE hangs on start today !

starting IDE , stays here:only kill with taskmanager possible.problem exist when starting IDE today, yesterday and before was no problem.yesterday i closed it as usual and shut down PC.today - no start. but when i choose other workspace, it is starti...

0693W00000aJG4aQAG.png
AScha.3 by Super User
  • 4700 Views
  • 2 replies
  • 4 kudos

Resolved! Can't compile X-Cube-Cellular TCP_Echo_Client example

Hi,I'm running STM32Cube 1.11.2 under Ubuntu 22.04While I can compile the TCP_Echo_Client_PPP example with no issue, I can't do the same with TCP_Echo_Client.The compilation issue is the tx_thread_schedule.s has undefined references to _tx_thread_sec...

GBeto.1 by Associate II
  • 2815 Views
  • 5 replies
  • 0 kudos