STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1558 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 590 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CMake 3.20 or higher is required

HI I try to import my Stm32cubeIde project into VSCodeI have install STM32CubeCLTthe configuration failed with this error [variant] Loaded new set of variants[kit] Successfully loaded 5 kits from C:\Users\XXXXXX\AppData\Local\CMakeTools\cmake-tools-k...

LHOUE by ST Employee
  • 4498 Views
  • 4 replies
  • 0 kudos

Host process of CDC (Virtual Port Com) does not work.

I am using STM32G0B1KC to make a CDC class USB Host.I selected in STM32CubeIDE, Mode=Host_Only (FS) in Connectivity - USB_DRD_FS and Communication Host Class (Virtual Port Com) in Middleware - USB_HOST.Before creating the user program, I checked the ...

JJ4IQV by Associate
  • 4222 Views
  • 7 replies
  • 0 kudos

Writing to flash bricks stm32G030 and stm32G031

If I create a program using stmcubeIDE and ADD the code below it bricks the processor . I gather in some way I am overwritting the bootloader that controls stlink and get the errorTarget no device foundError in initializing ST-LINK device.Reason: No ...

PGood.1 by Associate II
  • 2846 Views
  • 3 replies
  • 0 kudos

Debugging with GDB server localhost doesn't work

STM32CubeIDE for MAC Version: 1.12.0Just installed the tools and connected an STM32 Nucleo 144 for the first time.After connecting it, a ST-Link upgrade window popped up about updating the firmware of the board which I did. Got the Upgrade successful...

0693W00000bhQI5QAM.png
MMain.1 by Associate II
  • 3561 Views
  • 3 replies
  • 0 kudos

Resolved! X-CUBE-IAP-SD

The above designated code seems not to support STM32 CUBE IDE. It is based on the SW4STM32 and MDK-ARM platforms. Can anyone please direct me to the proper source? Or, is there a way to convert any of these to cube IDE? Thank you :folded_hands:​

RWeis.0 by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos

Resolved! Linker Options Tab Has Disappeared From Properties?

I used the Linker options to set optimization earlier today. Now, I no longer seem to have that tab in Project>Properties. Using the latest version of the IDE (1.12.0). I'm sure it's something dumb I did, but can't figure out how to get it back.

_legacyfs_online_stmicro_images_0693W00000bht1hQAA.png
nobbyv77 by Associate II
  • 1922 Views
  • 2 replies
  • 0 kudos