STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Implement error handling using Motor profiler API

Is there a Motor profiler API or any other tool that I can use to retrieve the error status from the ST Motor pilot programmatically? I'm interested in obtaining informations about the following errors:If it's not available, I would appreciate any al...

GJamo1_0-1687685234853.png
GJamo.1 by Associate II
  • 1871 Views
  • 1 replies
  • 0 kudos

Resolved! How to generate timer in STM32

Hello! Recently I have been working on ADC, where I connect a potentiometer to a bread board and by using jumper wires I  connect it with ARM Cortex M4, STM32G491. Thankfully I have received the outputs too. But the challenge is, I have to include ti...

stm32c011f6p6

Hello sir,  I used stm32cubeide  with stlink v2.   I tried to download the *.elf file to stm32c011f6p6 chip however, I have the error ====Open On-Chip Debugger 0.12.0-00017-gb153daa14 (2023-02-03-14:58) [https://github.com/STMicroelectronics/OpenOCD]...

choi1 by Associate
  • 2454 Views
  • 2 replies
  • 0 kudos

USB OTG with different connectors

Hello, everyone. I'm using the STM32F407IGT6 MCU.In my hardware, there are two USB connectors: USB A, for transferring/receiving data from a mass storage device, and USB B, for virtual communication with a PC.I would like to know if there is any way ...

Ade J.3 by Associate II
  • 869 Views
  • 0 replies
  • 0 kudos

Trouble with capturing sensor Data from si115x with an L432KC

Hey there,currently I am struggeling with capturing the sensor value from an si115x (Proximity & ambient light) Sensor.So far, this would be my code:void ReadSensorData(void){uint8_t sensorAddress = 0x53 << 1; // shift left to account for R/W bituint...

sasi by Associate
  • 1559 Views
  • 0 replies
  • 0 kudos

Content assist doesn't work with ctrl+space

My content assist does'nt work when I press ctrl+space but it's work when go to menu edit/content assist.Which parameter should I look ?I tried already In Preferences -> C/C++ -> Editor -> Content Assist -> AdvancedI checked the following boxes:Parsi...

Sebovernet_0-1687204625285.png