cancel
Showing results for 
Search instead for 
Did you mean: 

How to regenerate STM32CubeIDE project for FreeRTOS X-CUBE-CELLULAR version 7.1.0?

FCham.1
Associate II

Hi,

I am trying the project out of the box and it does not work. Either if I regenerate the project using MX or try to load it directly. Only the AzureRTOS version is working.

Any tips or help would be ver appreciated.

My ultimate goal is to download that project, run MX, generate the code (eventually modify some GPIO, ...), compile via STM32CubeIDE (Ideally VSCode) and launch.

Thank you very much!

Félix

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Rim LANDOLSI
ST Employee

Hello @Félix Champagne-Lapointe​ and welcome to the community,

I have successfully generated the code of one of the projects downloaded for  FreeRTOS X-CUBE-CELLULAR from this site. If I have understand well , you have errors in generating and compiling the code?

Could you provide the STM32CubeIDE and STM32CubeMX versions. Any additional information would be helpful!

Thanks,

Rim

FCham.1
Associate II

Yes, that is the issue. That would help me creating a new project from that example.

I tried both V7.1.0 and V7.0.0 and they both have compile issues after generation.

My STM32CubeIDE version is:

Version: 1.12.0

Build: 14980_20230301_1550 (UTC)

My STM32MX Version is: 6.8.0