STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 564 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Pointer to cyclic buffer at stm32H7A3

I am running ADC DMA in cyclic modeat STM32G474CET6  Im useingBuffer_Addr_At_Trigger[ ADC_Loop_Counter] = hdma_adc1.Instance->CNDTR;to read the pointer of the cyclic bufferIn the STM32H7 familyAn syntax error for CNDTRI can't find the appropriate reg...

hroze.1 by Associate II
  • 2006 Views
  • 3 replies
  • 1 kudos

NUCLEO-F756ZG ethernet CubeIDE configuration

Hello all!help needed! :)For last week I try to make UDP server on NUCLEO-F756ZG.I am stuck in the beginning...I can't configure my board to ping it.From reading old threads I understand that there was an issue with automatic ethernet configuration o...

AKhar.5 by Associate II
  • 3661 Views
  • 5 replies
  • 0 kudos

XCore407i

Estoy tratando de iniciar con la board XCore407I, descargue el ide ST32CubeIDE pero quiero generar un nuevo proyecto en Board Selector no esta XCore407I.Que puedo hacer???

Resolved! Preprocessor Macro file does not work for me

Hello EveryoneI'm trying to use Preprocessor Macro Files but they do not seem to work for me. I add the file path to a .h header with a couple of defines that I would like to use globally here.When I build the project, these defines are not found.Thi...

JWend1_1-1699266268853.png
JWend.1 by Associate II
  • 5565 Views
  • 8 replies
  • 1 kudos